This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用TM4C129x控制两片CC3100的驱动开发问题?

Other Parts Discussed in Thread: CC3100

你好,

       第一个问题:我看到TI-RTOS下的关于CC3100的驱动目前只支持一个WIFI 模块,我现在要用一片TM4X129X来控制两个CC3100,请问如何修改WIFI驱动来实现这个目的,谢谢?

第二个问题:TI-RTOS的WIFI3100的驱动是通过库的方式链接的,修改驱动相关代码必须重新编译库对吗?而且CCS不能对该库进行重编译,只能在DOS环境下编译,这样有一个问题,编译产生的错误无法查看,也不知道错误在哪,不知道对CC3100库的源文件进行修改重编译有什么方便的操作方法吗?谢谢。

  • CC3100的驱动程序可以看到底层的SPI或是UART的源码啊。

    如果你要控制两块CC3100的话,需要注意在TI-RTOS下面任务的建立和优先级的设置。

    谢谢

  • 我没有说看不到源码,我是说修改源码在ccs下编译不起作用,原因是CC3100这部分代码是以库的形式连接到工程中去的,必须重新编译库才
    行。我理解的对吗?谢谢!(我的工程是基于TI-RTOS下面TM4C129X的CC3100的例程开发的。)