Part Number: CC3235S
我现在用10块CC3235S的板子作为STA连接不同的AP设备时,有的会连接成功log输出IP和Gateway的地址,有的怎会有一部分连接不上地址显示为0。
STA失败时返回以下log信息。有6台设备成功了,4台失败了。我应该如何继续调查这种事情的真正原因。AP的最大连接数是64.
[NETAPP EVENT] IP Acquired: IP=10.255.254.235 , Gateway=0.0.0.0


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC3235S
我现在用10块CC3235S的板子作为STA连接不同的AP设备时,有的会连接成功log输出IP和Gateway的地址,有的怎会有一部分连接不上地址显示为0。
STA失败时返回以下log信息。有6台设备成功了,4台失败了。我应该如何继续调查这种事情的真正原因。AP的最大连接数是64.
[NETAPP EVENT] IP Acquired: IP=10.255.254.235 , Gateway=0.0.0.0


您好,
AP端的IP池是静态还是DHCP,IP地址是否耗尽,租期等。
STA端的固件版本都是一致的么?
抓 Log 看一下 AP 设备上的系统日志输出,确定一下是 STA 连接问题还是 IP 地址分配的错误。比如STA端是否有类似client can not connect:-114或者sl disconnect reason 200等