怎样提高WlanScan函数的扫描速度呀?现在是11秒扫描一次,好慢呀?求解
static long WlanScan(void *pvParameters)
{
long lRetVal = -1;
unsigned short ucIndex;
unsigned char ucpolicyOpt;
union
{
unsigned char ucPolicy[4];
unsigned int uiPolicyLen;
}policyVal;
InitializeAppVariables();
//
// Following function configure the device to default state by cleaning
// the persistent settings stored in NVMEM (viz. connection profiles &
// policies, power policy etc)
//
// Applications may choose to skip this step if the developer is sure
// that the device is in its default state at start of applicaton
//
// Note that all profiles and persistent settings that were done on the
// device will be lost
//
lRetVal = ConfigureSimpleLinkToDefaultState();
if(lRetVal < 0)
{
if (DEVICE_NOT_IN_STATION_MODE == lRetVal)
{
UART_PRINT("Failed to configure the device in its default state\n\r");
}
return lRetVal;
}
//UART_PRINT("Device is configured in default state \n\r");
//
// Assumption is that the device is configured in station mode already
// and it is in its default state
//
lRetVal = sl_Start(0, 0, 0);
if (lRetVal < 0 || ROLE_STA != lRetVal)
{
UART_PRINT("Failed to start the device \n\r");
return lRetVal;
}
//UART_PRINT("Device started as STATION \n\r");
//
// make sure the connection policy is not set (so no scan is run in the
// background)
//
ucpolicyOpt = SL_CONNECTION_POLICY(0, 0, 0, 0,0);
lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION , ucpolicyOpt, NULL, 0);
if(lRetVal != 0)
{
GPIO_IF_LedOn(MCU_EXECUTE_FAIL_IND);
UART_PRINT("Unable to clear the Connection Policy\n\r");
return lRetVal;
}
//
// enable scan
//
ucpolicyOpt = SL_SCAN_POLICY(1);
//
// set scan cycle to 10 seconds
//
policyVal.uiPolicyLen = 10;
//
// set scan policy - this starts the scan
//
lRetVal = sl_WlanPolicySet(SL_POLICY_SCAN , ucpolicyOpt,
(unsigned char*)(policyVal.ucPolicy), sizeof(policyVal));
if(lRetVal!=0)
{
GPIO_IF_LedOn(MCU_EXECUTE_FAIL_IND);
UART_PRINT("Unable to set the Scan Policy\n\r");
return lRetVal;
}
MAP_UtilsDelay(8000000);
//
// get scan results - all 20 entries in one transaction
//
ucIndex = 0;
//
// retVal indicates the valid number of entries
// The scan results are occupied in netEntries[]
//
lRetVal = sl_WlanGetNetworkList(ucIndex, (unsigned char)WLAN_SCAN_COUNT,
&netEntries[ucIndex]);
if(lRetVal==0)
{
GPIO_IF_LedOn(MCU_EXECUTE_FAIL_IND);
UART_PRINT("Unable to retreive the network list\n\r");
return lRetVal;
}
/* put a break point here and check netEntries[] value for scan ssid list */
//
// get scan results - 4 transactions of 5 entries
//
ucIndex = 0;
memset(netEntries, 0, sizeof(netEntries));
do
{
lRetVal = sl_WlanGetNetworkList(ucIndex,
(unsigned char)WLAN_SCAN_COUNT/4,
&netEntries[ucIndex]);
ucIndex += lRetVal;
}
while ((lRetVal == WLAN_SCAN_COUNT/4) && (ucIndex < WLAN_SCAN_COUNT));
/* put a break point here and check netEntries[] value for scan ssid list */
//
// disable scan
//
ucpolicyOpt = SL_SCAN_POLICY(0);
lRetVal = sl_WlanPolicySet(SL_POLICY_SCAN , ucpolicyOpt, NULL, 0);
if(lRetVal != 0)
{
GPIO_IF_LedOn(MCU_EXECUTE_FAIL_IND);
UART_PRINT("Unable to Clear the Scan Policy\n\r");
return lRetVal;
}
//UART_PRINT("SUCCESS\n\r");
return SUCCESS;
}