ti专员你好:
cc3100boost板上其他没动,只是把lash换成我买的AT45DB081E 8-Mbit的flash,格式化都不能成功?用uniflash软件操作,做什么都不成功。 ti生产的cc3100boost板上只能用跟它型号一样的flash芯片。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,请用我们推荐的FLASH 型号,在release notes里面有我们测试过的几种型号。其它的型号我们比较难保证。
Yonghua Pan 你好:
1、sFLASH (AT45DB081E)也是release notes里推荐的,
2、现在我们把CC3100BOOST上的XCC3100HZ换成了我们在得捷上买的CC3100R1,其他元件都是原版的,我们试着用UNIFLASH下载Format、Program、Service Pack等操作,出现如下错误:
[11:11:47] Begin Format operation.
[11:11:49] INFO: > Executing Operation: Connect
[11:11:51] INFO: setting break signal
[11:11:52] INFO: detecting FTDI for device reset
[11:12:07] ERROR: ---reading ACK signal failed---
[11:12:07] WARNING: ---seting break signal to false failed---
[11:12:09] INFO: setting break signal
[11:12:10] INFO: detecting FTDI for device reset
[11:12:26] ERROR: ---reading ACK signal failed---
需要怎样解决?(我这样试过2个新ic,问题是一样的)
3、我猜测我们买的CC3100R1是不是没有固件代码?如果需要新ic固件下载,需要什么设备?
谢谢!
Ken Wang你好:
首先谢谢你的回复,
由于我是直接在CC3100BOOST的板上焊上了我的CC3100R1,所以供电、RESET、nHIB都是TI默认条件。
现在我问题是:
1、新购置的芯片CC3100R1本身就是一个没有固件的芯片,是不是?
2、我在试的过程中,发现32K XTAL就没有起振,于是我使用了外部晶振,还是不能起振,按照SHEETDATA上第14页Figure 4-6. First-Time Power-Up and Reset Removal Timing Diagram (32K XTAL)的描述,32K XTAL起振是需要固件初始化之后才可以起振的,是这样吗?
3、如果芯片没有固件,我该用什么设备可以下载固件?
谢谢!