TI大神们,
我想在CC3200LP不进行smartconfig时,手机APP搜索不到设备,即关闭MDNS广播功能,只有当需要配置时,才开启广播功能,如何做到呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI大神们,
我想在CC3200LP不进行smartconfig时,手机APP搜索不到设备,即关闭MDNS广播功能,只有当需要配置时,才开启广播功能,如何做到呢?
\brief Stops a network application
Gets and stops network application for the current WLAN mode
\param[in] AppBitMap application id, could be one of the following: \n
- SL_NET_APP_HTTP_SERVER_ID
- SL_NET_APP_DHCP_SERVER_ID
- SL_NET_APP_MDNS_ID
\return On error, negative number is returned
\sa
\note This command disables the application for the current active WLAN mode (AP or STA)
\warning
\par Example:
\code
For example: Stopping internal HTTP server:
sl_NetAppStop(SL_NET_APP_HTTP_SERVER_ID);
\endcode
*/
#if _SL_INCLUDE_FUNC(sl_NetAppStop)
_i16 sl_NetAppStop(const _u32 AppBitMap);
您好,谢谢您的回答,只是关于这个封装函数的功能,我知道是可以关闭MDNS功能,但是它所关闭掉的是整个Socket通路,导致CC3200LP其他的网络服务功能难以实现,也并不能解决我所说的一键配置完成后关闭MDNS广播功能,而不对其他功能造成影响的初衷,所以我不打算用这个函数,不过还是谢谢您的回答,目前通过其他方式已经解决问题了。