cc3200 serial wifi 例程,两块板子成功连接到AP上,
如何相互收发数据? 用send recv命令? 如果知道各个板子的IP地址?
PING 百度的IP地址,也没有反应?
*************************************************
CC3200 SERIAL WiFi Application
*************************************************
Host Driver Version: 1.0.0.1
Build Version 2.4.0.2.31.1.3.0.1.1.0.3.34
Device is configured in default state
Started SimpleLink Device: STA Mode
>>>
>>>
>>> Attempting to auto connect to AP
>>> Attempting to acquire IP
>>>
>>> Connection Unsuccessful.
>>> Connect to the AP using local control mode(\\<)
>>> [WLAN EVENT] STA Connected to the AP: Tu , BSSID: 2:1a:11:f6:fa:bc
Entered INTERPRETER mode
>>> li
>>> 123456789
>>> ping 202.108.22.103