CC3200站点已经接入路由,然后怎么操作,能建立一个httpsever
我把lRetVal = ConnectToNetwork();改为站点连接服务器的函数,其它没怎么变,输入站点IP,打不开网页,希望高手指点一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC3200站点已经接入路由,然后怎么操作,能建立一个httpsever
我把lRetVal = ConnectToNetwork();改为站点连接服务器的函数,其它没怎么变,输入站点IP,打不开网页,希望高手指点一下
/*!
\brief Internal function for setting network application configurations
\return On success, zero is returned. On error, -1 is
returned
\param[in] AppId Application id, could be one of the following: \n
- SL_NET_APP_HTTP_SERVER_ID
- SL_NET_APP_DHCP_SERVER_ID
- SL_NET_APP_MDNS_ID
- SL_NET_APP_DEVICE_CONFIG_ID
\param[in] SetOptions set option, could be one of the following: \n
- SL_NET_APP_DHCP_SERVER_ID
- NETAPP_SET_DHCP_SRV_BASIC_OPT
- SL_NET_APP_HTTP_SERVER_ID
- NETAPP_SET_GET_HTTP_OPT_PORT_NUMBER
- NETAPP_SET_GET_HTTP_OPT_AUTH_CHECK
- NETAPP_SET_GET_HTTP_OPT_AUTH_NAME
- NETAPP_SET_GET_HTTP_OPT_AUTH_PASSWORD
- NETAPP_SET_GET_HTTP_OPT_AUTH_REALM
- NETAPP_SET_GET_HTTP_OPT_ROM_PAGES_ACCESS
- SL_NET_APP_MDNS_ID
- NETAPP_SET_GET_MDNS_CONT_QUERY_OPT
- NETAPP_SET_GET_MDNS_QEVETN_MASK_OPT
- NETAPP_SET_GET_MDNS_TIMING_PARAMS_OPT
- SL_NET_APP_DEVICE_CONFIG_ID
- NETAPP_SET_GET_DEV_CONF_OPT_DEVICE_URN
- NETAPP_SET_GET_DEV_CONF_OPT_DOMAIN_NAME
\param[in] OptionLen option structure length
\param[in] pOptionValues pointer to the option structure
\sa
\note
\warning
\par
\code
Set DHCP Server (AP mode) parameters example:
SlNetAppDhcpServerBasicOpt_t dhcpParams;
_u8 outLen = sizeof(SlNetAppDhcpServerBasicOpt_t);
dhcpParams.lease_time = 4096; // lease time (in seconds) of the IP Address
dhcpParams.ipv4_addr_start = SL_IPV4_VAL(192,168,1,10); // first IP Address for allocation. IP Address should be set as Hex number - i.e. 0A0B0C01 for (10.11.12.1)
dhcpParams.ipv4_addr_last = SL_IPV4_VAL(192,168,1,16); // last IP Address for allocation. IP Address should be set as Hex number - i.e. 0A0B0C01 for (10.11.12.1)
sl_NetAppStop(SL_NET_APP_DHCP_SERVER_ID); // Stop DHCP server before settings
sl_NetAppSet(SL_NET_APP_DHCP_SERVER_ID, NETAPP_SET_DHCP_SRV_BASIC_OPT, outLen, (_u8* )&dhcpParams); // set parameters
sl_NetAppStart(SL_NET_APP_DHCP_SERVER_ID); // Start DHCP server with new settings
\endcode
\code
Set Device URN name example:
Device name, maximum length of 33 characters
Device name affects URN name, own SSID name in AP mode, and WPS file "device name" in WPS I.E (STA-WPS / P2P)
In case no device URN name set, the default name is "mysimplelink"
Allowed characters in device name are: 'a - z' , 'A - Z' , '0-9' and '-'
_u8 *my_device = "MY-SIMPLELINK-DEV";
sl_NetAppSet (SL_NET_APP_DEVICE_CONFIG_ID, NETAPP_SET_GET_DEV_CONF_OPT_DEVICE_URN, strlen(my_device), (_u8 *) my_device);
\endcode
*/
#if _SL_INCLUDE_FUNC(sl_NetAppSet)
_i32 sl_NetAppSet(const _u8 AppId ,const _u8 Option,const _u8 OptionLen,const _u8 *pOptionValue);
#endif