This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 ADC问题

Other Parts Discussed in Thread: CC3200

您好,请问CC3200的ADC采样频率可以设置吗? 我翻了半天API还有手册,并没有设置的地方

设置ADC管脚后,拿示波器观察ADC引脚,发现是62.5K Hz的脉冲,这个对信号采样有影响吗?

谢谢!

  • Hi Weicheng,

    您好!

    关于CC3200的ADC sample rate,确实没法设置,是固定的62.5KSPS。 谢谢!

  • Voltage is 0.557471

    Voltage is 0.573877

    Voltage is 0.578662

    Voltage is 0.575244

    Voltage is 0.560547

    Voltage is 0.574561

    Voltage is 0.573535

    Voltage is 0.559863

    Voltage is 0.559521

    Voltage is 0.555420

    Command Usage 
    -------------- 
    adcdemo <adc_inputpin>

    Parameters 
    -------------- 
    adc_inputpin - Pin to which Analog signal is connected [58|59|60] 
    -------------------------------------------------------------------------

    用的是官方给的sdk例程里面的adc

    我没有接任何输入信号,但其adc采集有电压是有的

    这是怎么回事

    请技术人员给出解答