This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3200使用TI-RTOS,创建任务扫描网络不能获取正确的RSSI



使用cc3200例程scan-polic可以扫描网络,能够获取正确的ssid和rssi,但当使用TI-RTOS时,创建任务运行WlanScan时,不能获取正确的RSSI,而ssid第一个是对的,下面的都是空的。请TI的专家指导下,谢谢!!

main函数如下:硬件初始化代码略去

lRetVal = VStartSimpleLinkSpawnTask(SPAWN_TASK_PRIORITY);
if(lRetVal < 0)
{
      ERR_PRINT(lRetVal);
     Message(" VStartSimpleLinkSpawnTask error\r\n");
     LOOP_FOREVER();
}
lRetVal = osi_TaskCreate(WlanScan,(const signed char *)"wlan",OSI_STACK_SIZE,NULL,1,NULL );
if(lRetVal < 0)
{
       ERR_PRINT(lRetVal);
       Message(" osi_TaskCreate error\r\n");
       LOOP_FOREVER();
}
osi_start();

}

扫描函数如下:

void WlanScan(void *pvParameters)
{

      long lRetVal = -1;

      unsigned short ucIndex;
      unsigned char ucpolicyOpt;
      union
     {
          unsigned char ucPolicy[4];
          unsigned int uiPolicyLen;
      }policyVal;
      InitializeAppVariables();

      lRetVal = ConfigureSimpleLinkToDefaultState();
      if(lRetVal < 0)
      {
           if (DEVICE_NOT_IN_STATION_MODE == lRetVal)
          {
               UART_PRINT("Failed to configure the device in its default state\n\r");
           }

      }

      UART_PRINT("Device is configured in default state \n\r");

      lRetVal = sl_Start(0, 0, 0);
      if (lRetVal < 0 || ROLE_STA != lRetVal)
      {
            UART_PRINT("Failed to start the device \n\r");

       }

       UART_PRINT("Device started as STATION \n\r");

       ucpolicyOpt = SL_CONNECTION_POLICY(0, 0, 0, 0,0);
       lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION , ucpolicyOpt, NULL, 0);
       if(lRetVal != 0)
      {
             UART_PRINT("Unable to clear the Connection Policy\n\r");

       }

       ucpolicyOpt = SL_SCAN_POLICY(1);

        policyVal.uiPolicyLen = 10;

        lRetVal = sl_WlanPolicySet(SL_POLICY_SCAN , ucpolicyOpt,(unsigned char*)(policyVal.ucPolicy), sizeof(policyVal));
        if(lRetVal!=0)
       {
              UART_PRINT("Unable to set the Scan Policy\n\r");

        }
        MAP_UtilsDelay(8000000);
        while(1)

       {
               ucIndex = 0;
               memset(netEntries, 0, sizeof(netEntries));

               lRetVal = sl_WlanGetNetworkList(ucIndex, (unsigned char)WLAN_SCAN_COUNT,&netEntries[ucIndex]);
               if(lRetVal==0)
              {

                     UART_PRINT("Unable to retreive the network list\n\r");
               }

              for(ucIndex=0;ucIndex<lRetVal;ucIndex++)
             {
                      UART_PRINT("ssid:%s\n\r",netEntries[ucIndex].ssid);
                      UART_PRINT("rssi:%d\n\r",netEntries[ucIndex].rssi);
              }

             MAP_UtilsDelay(8000000);
      }

}