This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI CC3200高速传输模式

Other Parts Discussed in Thread: CC3200

Hi TI技术人员你们好,

我购买了你们的WiFi CC3200的板子,而我想用来传输大量的资料,我在Sample code里有看到UART/I2C/SPI的example code,请问你们两个问题.

1. 你们有支援USB或是SDIO模式的传输模式吗? 如果有的话,传输资料的速度会比UART/I2C/SPI来的快吗?

2.USB或是SDIO模式的传输模式是否有example code可以参考?

  • 没有USB, 可以有1线的SDIO。你是要做什么样的产品呢?

  • 我要做的产品功能CC3200连接STM32的板子,而主程序是写在STM32上,CC3200只是用来与另一台Server的电脑进行WiFi的连线进行传输功能而己.
    如果使用UART或是SPI,进行传输的话,速度会比较慢,因此,想说STM32与CC3200的沟通接口使用1线的SDIO模式来进行的的速度应该会比较快.
    因此,请帮忙确认下列三点.
    1.如果STM32与CC3200的沟通接口使用1线的SDIO模式来进行大数据传输的话,传输速度会比UART或是SPI还要快吗?
    2.你们有使用UART/I2C/SPI/1线的SDIO之间Throughput的数值比较结果吗?
    3.1线的SDIO模式有对应的example code与SDIO的接线脚位图呢?