This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3XXX系列传输距离

Other Parts Discussed in Thread: CC2592

请教下专家CC3XXX系列传输距离相关问题,如CC3000,接收灵敏度为-91dBm,最大发射功率为17dBm,收发天线增益都按2.1dB来算,按照Friss公式算出距离为5249.8m,为啥说CC3XXX的室内通信距离为75m,室外距离是250m,这么大的距离落差,直接制约因素都有哪些?另外,ti的excel range 测试工具貌似可以对CC3XXX进行评估。此外,CC2592作为2.4GHz的range extender能否用于CC3XXX?如果不能直接用,那这range extender 除了跟频段有关,还受别的什么因素影响?频段不同,直接会影响哪些设计。最后,想请教下ti有专门的基带处理芯片和专门的组网芯片么?