This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100的固件是写在芯片内部还是写在外部FLASH中?

Other Parts Discussed in Thread: CC3100, CC3100BOOST

如题。

我把在CC3100BOOST板上升级好的CC3100芯片取下来,再焊到自己的电路板上,(因为第一版电路的设计问题,不能直接在上面升级,只好这么做)程序走到 :retVal = sl_WlanPolicySet(SL_POLICY_CONNECTION, SL_CONNECTION_POLICY(1, 0, 0, 0, 1), NULL, 0);时,返回值会是-7,查论坛之前的帖子,说-7表示需要再升级固件,我们试了几次都是这种结果。但是我们把在CC3100BOOST上面升级过的CC3100和FLASH同时取下来,再焊到电路板上,sl_WlanPolicySet的返回值就是正确的了。这是不是表示固件是写在FLASH里面的?

但是CC3100和FLASH同时换过来之后,在与AP建立连接的while((!IS_CONNECTED(g_Status)) || (!IS_IP_ACQUIRED(g_Status)))处,一直死循环跳不出来了,请问这又是什么原因?