各位大侠和TI老师:你们好!
使用CC3200 LUNCHXL开发板,下载CC3200SDK_1.1.0中的P2P样例,运行以后,终端出现如下信息
*************************************************
CC3200 P2P Demo Application
*************************************************
Scan Wi-FI direct device in your handheld device
Host Driver Version: 1.0.0.10
Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3
Device is configured in default state
Started SimpleLink Device: P2P Mode
Error [-7] at line [920] in function [P2PConfiguration]
Setting P2P configuration failed
为什么会这样。blinky 和 wlan_station 运行正常。希望给点提示,谢谢。