This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200的电源问题

Other Parts Discussed in Thread: CC3200

我使用CC3200芯片自己设计了一个实验板,宽电压供电的模式,3.3V输入,AN_POWER,PA_POWER,DIG_POWER由内部的DCDC产生,板子焊好后进行调试,Pin36,Pin25 LDO_IN1,LDO_IN2,电平在1.9V用示波器看直流电平没有规律的会跌落到地持续时间8ms左右,Pin9(VDD_DIG),Pin56(VDD_DIG)电平在1.2V用示波器看直流电平没有规律的也会跌落的情况,但是没有跌落到地持续时间和PIN36对应,PIN33(VDD_PA_IN)上没有电压。查看40M和32K晶振的波形也是如此,不是连续完整的波形,也一段时间不震荡,时间和PIN36对应。PIN24(VDD_PLL)没有电平,PIN49(VDD_RAM) 也有跌落的波形,时刻和PIN36对应。无法连接Jlink。不知道是什么原因?