TI员工:
你们好,现在我想使用3200的SPI接口(GPIO00-***,GPIO15-MIBO,GPIO16-MOBI,GPIO14-***)操作外部FLASH,我选用的IC是W25Q64B,但是通过更改sdk中自带的SPI-DEMO发现写进去,读出来没有数据,观测到MAP_SPITransfer的返回值为0,按照头文件中的说明,返回0表示成功,但是为什么读出来没有数据,是对FLASH的型号有要求吗,还是其中的某个函数参数需要注意,W25Q64B用的是标准的SPI接口,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI员工:
你们好,现在我想使用3200的SPI接口(GPIO00-***,GPIO15-MIBO,GPIO16-MOBI,GPIO14-***)操作外部FLASH,我选用的IC是W25Q64B,但是通过更改sdk中自带的SPI-DEMO发现写进去,读出来没有数据,观测到MAP_SPITransfer的返回值为0,按照头文件中的说明,返回0表示成功,但是为什么读出来没有数据,是对FLASH的型号有要求吗,还是其中的某个函数参数需要注意,W25Q64B用的是标准的SPI接口,谢谢。
请问你用FLASH有什么用的,其实CC3200外挂的那个FLASH你也是可以部分操作的。它可以满足你的需要吗?