Other Parts Discussed in Thread: CC3351
am6254的设备树配置 SDIO(MMC2) 与 cc3351连接,
wifi_pins_default: wifi-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x0120, PIN_INPUT, 0) /* (C24) MMC2_CMD */
AM62X_IOPAD(0x0118, PIN_INPUT, 0) /* (D25) MMC2_CLK */
AM62X_IOPAD(0x0114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */
AM62X_IOPAD(0x0110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */
AM62X_IOPAD(0x010c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */
AM62X_IOPAD(0x0108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */
AM62X_IOPAD(0x0124, PIN_INPUT, 0) /* (A23) MMC2_SDCD */
AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */
>;
};
wifi_en_pins_default: wifi-en-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x009c, PIN_OUTPUT, 7) /* (V25) GPMC0_WAIT1.GPIO0_38 */
>;
};
外接3.3V电压,实际测量CC3351的SDIO接口各个引脚电平值
Vcc = 3.3V
(C24) MMC2_CMD = 0.5V
(D25) MMC2_CLK = 0.5V
(B24) MMC2_DAT0 = 0.5V
(C25) MMC2_DAT1 = 0.5V
(E23) MMC2_DAT2 = 0.5V
(D24) MMC2_DAT3 = 0.5V
IRQ_WL = 0.5V
RESET = 3.3V
GND = 0V
上面出现0.5V的电压值,不知道是什么原因引起的异常。