This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 开启网络处理器(NWP)重启!!!

Other Parts Discussed in Thread: CC3200

使用cc3200有一段时间了,前后做过2块板子。

均出现在sl_Start中开启NWP 时重启的情况。  /*HWREG(0x44025118) = 1*/ 

第一块板通过将500mA电源换成1A解决了这个问题,但第二块板使用1A DC/DC电源依然无法打开NWP。

另外使用TI官方的评估板,只使用500mA USB电源也无法打开NWP。

这个问题已经卡了很久,希望尽快给出答复。

之前看过有类似的帖子说是layout的问题,我们的方案采用的是四层板,布局比较紧凑,希望能给出解决方案。