Other Parts Discussed in Thread: UNIFLASH, , CC3100,
链接there seems to be an error when trying to retrieve deivce information.this means the device may not have been flashed with the proper FW or application(if using3220),and thus radio testing may not function properly.Please check and make sure your board is flashed with the correct FW and application.For more information,please refer to the wiki page for instruction. 跳出此失败,
板子是CC3200-LAUNCHXL,
CCS UniFlash
Version: 3.4.1.00012
使用的radiotool工具:CC3100_CC3200_RadioTool_1.2
SDK Version:CC3200SDK_1.5.0
servicepack:servicepack_1.0.1.15-2.15.0.1.bin
使用的C:\ti\CC3100_CC3200_RadioTool_1.2\CC3200BoardApplication_Binary/radiotool.bin。 请问是哪里出错了