麻烦问下,CC3200的 1.85V模式,用1.8V可以吗,1.85还得用电阻去调,1.8V有TPS73218直接OK。另外,如果不用这个模式的话,给CC3200接上BAT,是不是可以从DCDC_ANA1获得1.8V的电压给其他片子供电?这个电压稳吗,噪声多吗,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yuan,
Preregulated 1.85 V 1.76 1.85 1.9 V
最小值1.76V。1.8V就是太危险了, 稍微有纹波就挂了。 所以定了个1.85V.
2. 不可以给别人用的。影响cc3xxx本身的性能的。另外,这个dcdc的模式也会随cc3xxx的状态而变的。
BR. AZ