This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: 在声明自定义集群的时候出现的问题

Part Number: CC2340R5

[21]warning #10229-D: output section ".data" refers to load symbol "zb_zcl_custom_attr_init_server" and hence cannot be compressed; compression "lzss" is ignored

[22] undefined first referenced
[23] symbol in file
[24] --------- ----------------
[25] zb_zcl_custom_attr_init_server .\{AEE49B66-E8FA-43F8-929E-4851DBA4B67B}

[26]error #10234-D: unresolved symbols remain
[27]error #10010: errors encountered during linking; "reader.out" not built
[28]tiarmclang: error: tiarmlnk command failed with exit code 1 (use -v to see invocation)
[29]gmake[1]: *** [makefile:149: reader.out] Error 1
[30]gmake: *** [makefile:143: all] Error 2
[31]**** Build Finished

这个问题是如何解决?