Other Parts Discussed in Thread: CC2530
TI大神好,
最近自己做远程无线升级,使用的是芯片是cc2530,内存大小为256K,代码主要分boot和app两个部分,app代码的存储地址是通过修改lnk51ew_CC2530F256_banked.xcl的D_NEAR_CODE_START来确定起始地址:
-D_NEAR_CODE_START=0x0800 //将App起始地址设置为0x800
想请教下,是否可以将app代码放入BANK1中存储,然后由BANK0中的boot程序直接跳到0x8000以上执行app程序?
如果可以,该如何设置?还是修改D_NEAR_CODE_START的值吗?但是我修改D_NEAR_CODE_START=0x18000,出现了错误
初次接触,还望大神们指明方向,非常感谢!