如题,现在有一个协调器,一个终端设备,我想通过link key 来做组网控制,也就是说终端的link key和协调器有着相同的link key才能加入网络,否则 不能加入网络。。。请问可以实现么,另外我做了一下这个实验,实验条件是我修改了默认的DEFAULT_TC_LINK_KEY,根据抓包情况,不知道终端有没有加入网络,请ti工作人员帮忙分析一下
该怎么去配置这些参数 比如:
/*********************************************************************
* SECURITY GLOBAL VARIABLES
*/
// If TRUE, preConfigKey should be configured on all devices on the network
// If false, it is configured only on the coordinator and sent to other
// devices upon joining.
uint8 zgPreConfigKeys = FALSE;
// The type of link key in use. This will determine the security
// policies associated with sending and receiving APS messages.
// If ZG_GLOBAL_LINK_KEY APS TCLK security may be used for specific APS commands
// If ZG_UNIQUE_LINK_KEY APS TCLK security is required for specific APS commands
uint8 zgApsLinkKeyType = ZG_GLOBAL_LINK_KEY;
DEFAULT_TC_LINK_KEY