This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 终端 通过AF_DataRequest方法发包给协调器, 协调器在afIncomingMSGPacket_t 中是不是获取不到终端的ieee mac地址?
2. 我想获取源设备的物理地址,能不能在接收到源设备信息的时候获取到他的物理地址?
3. 请问下各位大神,有没什么方法获取源设备的物理地址?
VV你好,
我使用ZDP_IEEEAddrReq()函数确实能找到对应的MAC地址,可是我发现另一个很严重的问题。
我使用此函数定时进行查找MAC,可是过一段时间之后,设备就出现异常,无法发送点播数据出去。抓包中可以看到,Link_status_list中,各个短地址都显示IC=0,OC=0.在其他路由设备的Link_status_list中,此设备的IC=0,OC=0.
在附加:网络异常抓包4.psd文件中,有记录短地址为0xA73B的设备从正常到异常的情况,请VV大神帮我分析下具体原因?谢谢!
网络异常抓包4.psd文件中,0xA73B使用ZDP_IEEEAddrReq()函数定时每30秒轮流对地址为0x7B38和0x09E7的路由设备进行MAC地址查询。在抓包文件的第6824条信息开始,网络就出现异常,原来IC=1,OC=1,变成IC=1,OC=0,最后两个值都为0,然后就不能进行点播,也不会广播Link_status_list信息。可是0x09E7对0xA73B进行点播的时候,0xA73B又是可以收到点播信息的。
网络异常抓包3.psd文件是 网络异常抓包4.psd 完整的抓包信息,网络异常抓包4.psd 是过来了显示源地址的。
虽然不能进行点播,可是当设备发送广播信息的时候,它的网络又恢复正常了,ZDP_IEEEAddrReq()函数也能正常点播,Link_status_list信息也恢复正常广播,且所有IC=1,OC=1。
网络异常抓包7.psd文件中,是0xA73B进行广播数据后,网络恢复正常的抓包数据。从第118条抓包信息开始,网络慢慢恢复正常。
在此之前,我们的产品出现匹配数据丢失的现象,在这之前,我以为是FLASH的存储问题,或者是目的地址发生改变,现在我想,就是这个原因造成的,因为产品已经卖出去,在客户家里使用着,可是这个网络问题的出现,造成的后果很严重,所有请VV帮帮忙,分析下是什么原因?是不是协议栈的问题?我使用的协议栈是ZStack-CC2530-2.5.1a。
谢谢!