This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

nwk link status的作用

Other Parts Discussed in Thread: Z-STACK

抓包发现节点周期性发出nwk link status,这个广播包的作用是什么?在大量节点的网络中,每个节点都发出是否会造成网络堵塞?如果堵塞,如何去掉?谢谢

  • 如下是解释,from z-stack developer guide,简单讲,pro协议必须使用,路由设备没有周期性收到来自邻居的Link status,会把这个邻居移除。

    可以改变发送频率,但不能移除。大量节点的情况,参考: http://www.ti.com/lit/an/swra427c/swra427c.pdf

    9.7 Asynchronous Links
    An asynchronous link occurs when a node can receive packets from another node but it can’t send packets to that node. Whenever this happens, this link is not a good link to route packets.
    In ZigBee PRO, this problem is overcome by the use of the Network Link Status message. Every router in a ZigBee PRO network sends a periodic Link Status message. This message is a one hop broadcast message that contains the sending device’s neighbor list. The idea is this – if you receive your neighbor’s Link Status and you are either missing from the neighbor list or your receive cost is too low (in the list), you can assume that the link between you and this neighbor is an asynchronous link and you should not use it for routing.
    To change the time between Link Status messages you can change the compile flag NWK_LINK_STATUS_PERIOD, which is used to initialize _NIB.nwkLinkStatusPeriod. You can also change _NIB.nwkLinkStatusPeriod directly. Remember that only PRO routers send the link status message and that every router in the network must have the same Link Status time period.
    _NIB.nwkLinkStatusPeriod contains the number of seconds between Link Status messages.
    Another parameter that affects the Link Status message is _NIB.nwkRouterAgeLimit (defaulted to NWK_ROUTE_AGE_LIMIT). This represents the number of Link Status periods that a router can remain in a device’s neighbor list, without receiving a Link Status from that device, before it becomes aged out of the list. If we haven’t received a Link Status message from a neighbor within (_NIB.nwkRouterAgeLimit * _NIB.nwkLinkStatusPeriod), we will age the neighbor out and assume that this device is missing or that it’s an asynchronous link and not use it.

  • 也就是移除僵尸节点,协议栈本身有这个功能吗?我看到我们的程序里面自己添加了移除僵尸节点功能