Other Parts Discussed in Thread: CC2531, Z-STACK, CC2531EM-IOT-HOME-GATEWAY-RD
最近一直在弄这个程序来实现对ZLL灯的控制,之前调不通,现在终于都能弄好了,看了看代码,但是还有些问题一直不太明白。
1、这个应用用的是2531DONGLE,我看到灯控命令通过客户端程序(比如devlist)生成后通过socket发给server(zbcontroller.c),server接到后进行一些处理和解析后,最后是以一个字符数组的形式写给dongle的,然后不同的命令对应的字符数组不同。我想知道的是,这里的字符数组在进到dongle后,2531还要在解析一遍然后加工成zigbee的帧格式发走么,还是这里的数组不作处理了,只是直接通过zigbee协议栈走天线发出去了?换句话说,我想知道的是这里的字符数组是如何约定的,是符合ZLL某个标准的还是只是一个非标的协定。
2、DONGLE内才运行zstack,整个协议的实现都在这里,那作为server的beaglebone以及gateway的整个程序是不是可以说与zigbee本身的关系并不大,只是需要满足ZLL最上层的一些控制命令的种类和协定就可以?我想问,是不是不修改2531内的程序,单纯修改这个GATEWAY程序是无法实现控制ZLL灯以外的功能;想要干别的事儿就只能两方一同修改才行?
3、这个2531上的协议栈和zigbee中关于协调器、组网等有关系吗,对于应用开发者来说,是不是不需要关心这个协调器组网、添加终端之类的事情,协议栈自会实现,我们只需要知道设备地址(就像IP地址一样的东西),利用这个协议栈就能够实现数据收发了?
4、最后,关于这个灯控标准,是不是其实和ZIGBEE的关系并不是很大,更多的是个灯控的命令协议,也就是说这个命令只是通过zigbee这样的一个通信方式在两个设备之间传递而已;或者我可不可以说,其实这个灯控标准也完全可以用在蓝牙或者其他通信的协议之上?(其实自己现在属于一头雾水,可能问题不专业,还望大神不要鄙视)
这里是一段命令的字符数组的代码
void zbSocSetState(uint8_t state, uint16_t dstAddr, uint8_t endpoint,
uint8_t addrMode)
{
uint8_t cmd[] =
{ 0xFE, 11, /*RPC payload Len */
0x29, /*MT_RPC_CMD_AREQ + MT_RPC_SYS_APP */
0x00, /*MT_APP_MSG */
0x0B, /*Application Endpoint */
(dstAddr & 0x00ff), (dstAddr & 0xff00) >> 8, endpoint, /*Dst EP */
(ZCL_CLUSTER_ID_GEN_ON_OFF & 0x00ff), (ZCL_CLUSTER_ID_GEN_ON_OFF & 0xff00)
>> 8, 0x04, //Data Len
addrMode, 0x01, //0x01 ZCL frame control field. (send to the light cluster only)
transSeqNumber++, (state ? 1 : 0), 0x00 //FCS - fill in later
};
calcFcs(cmd, sizeof(cmd));
zbSocTransportWrite(cmd, sizeof(cmd));
}