This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ZDP_BindReq 绑定 的问题

Other Parts Discussed in Thread: Z-STACK

关于ZDP_BindReq 绑定 的问题
协议:Z-Stack Home 1.2.2a.44539
网络:一个协调器、两个终端等组成
希望C控制B
情况如下:
ClusterID: 0x0500
A:协调器
IEEE:0x00124B00028A3AA5
short:0x0000

B:终端
IEEE:0x00124B0002EFD3B6
short:0xDAD3
ENDPOINT:0x16

C:终端
IEEE:0x00124B00028A6334
short:0x7F07
ENDPOINT:0x11


在协调器上
在PC上通过Z-tool 2.0连接协调器串口 发送ZDO_BIND_REQ
(通过Z-tool 2.0连接协调器串口发送其他命令正常使用,也可以证明设备都是入网的。)
MT_ZDO_BIND_REQ:
<TX>02:45:31.7 COM9 ZDO_BIND_REQ (0x2521)
DstAddr: 0x7F07
SrcAddress: 0x00124B00028A6334
SrcEndpoint: 0x11
ClusterID: 0x0500
BindAddrMode: 0x02 (ADDRESS_16_BIT)
BindAddr: ........ (0xDA, 0xD3, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00)
BindEndpoint: 0x16


经过上面设置C不能控制B(整个系统使用EZMode,是可以入网、绑定和控制的)