This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530 ZigBee 和 cc3200 WiFI 2.4G 干扰如何解决?

Other Parts Discussed in Thread: Z-STACK

请教一下大家, 我们在做一个小产品, 有一个主机, 首先要通过ZigBee获取和控制终端,其次是要通过WiFi和外界交互。 但是两个都是2.4G, 会存在干扰。

我在网上找了一些解决方法:

1、分时去使用2530 和 3200,  但2530 要一直处于接收状态 去响应终端请求, 3200也是需要处于接收状态 去看手机端有没有请求。。

      这样好像就不能分时去调度了

2、让ZigBee 和 WiFi 用2.4G 不同的信道。 我ZigBee用的是ZStack-CC2530-2.5.1a,  好像z-stack 好像自己就会去扫描信道,去选择合适信道。 但好像也受到了      干扰

请教一下,这个问题,该如何解决。

  • 借鉴一下TI E2E 给出的答案

    https://e2e.ti.com/support/wireless_connectivity/simplelink_wifi_cc31xx_cc32xx/f/968/p/504812/1837595

    The WiFi has collision avoidance mechanism that is used to avoid interference. There are already multiple products operating in the same band without any coexistence issues. The air interface takes care of that. However simultaneous transmission in the same channel would cause issue and would ask for re-transmission. WiFi protocol would automatically perform a re-transmission in case of a missed packet. So this is already taken care.