This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2674P10: The CC2674P10's maximum communication distance is 20dBm.

Part Number: CC2674P10

Hi everyone:

I purchased the CC2674P10 chip and designed a PCB development board (20dBm RF circuit). I compiled the firmware based on TI's official ZNP example, then flashed the firmware to the development board. I connected the development board as a Zigbee adapter to Zigbee2MQTT, added a Zigbee device using Zigbee2MQTT, and then started testing the control distance.

When the distance between the Zigbee device and the development board exceeds 200 meters, Zigbee2MQTT cannot control the Zigbee device.

What is the maximum communication distance officially tested by TI?