如题,对协调器进行操作,不通过终端,便可获取协调器所管理的终端数量以及对应的短地址?急求!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是协调器自己管理的终端吗? 全网的,参考VV那个
static void CheckAddr(void) {
for (uint8 x=0;x<NWK_MAX_DEVICES;x++) {
byte nr = AssociatedDevList[x].nodeRelation;
if (nr == CHILD_RFD) {
//终端节点地址,数量可在此统计
//AssociatedDevList[x].shortAddr
}}}
typedef struct
{
uint16 shortAddr; // Short address of associated device
uint16 addrIdx; // Index from the address manager
byte nodeRelation;
byte devStatus; // bitmap of various status values
byte assocCnt;
byte age;
linkInfo_t linkInfo;
aging_end_device_t endDev;
uint32 timeoutCounter;
bool keepaliveRcv;
} associated_devices_t;