您好,我手头有一个CC2538DK开发板,看CC2538的介绍中,支持Over-the-Air Upgrade and Download,但是没能找到更多介绍。有没有详细一些的介绍或者示例程序可供参考?感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Z-Stack Home 1.2.2a已安装,按照文档所说进行配置,里面3.2.2.1的Step1B中的SampleAPP.eww没有找到,是Z-Stack Home中的文件吗?
此外,我用CC2538DK套件,用SmartRF06连接到电脑,在Step3的时候,3)和4)都报错,提示如下:
Thu Jun 23, 2016 22:22:21: Fatal error: Could not open the emulator board file: Check the project settings Session aborted!
Thu Jun 23, 2016 22:22:21: Failed to load flash loader: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\flashloader\TexasInstruments\FlashCC2538RAM32K.flash
您看这可能是什么原因?该如何解决呢?谢谢