This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教ZHA1.2.2协议栈如何修改发射功率

Other Parts Discussed in Thread: CC2530, Z-STACK

你好!

   请教一下,在ZHA1.2.2协议栈里如何修改发射功率?

谢谢!

  注:Z-Stack Home 1.2.2协议栈,CC2530芯片,不加无线功放(PA)

  •   value=3;

    MAC_MlmeSetReq( MAC_PHY_TRANSMIT_POWER_SIGNED,&value);

    或者

    ZMacSetReq(MAC_PHY_TRANSMIT_POWER_SIGNED,&value)

    value的值参考如下,最大3,最小-22

    const uint8 CODE macRadioDefsTxPwrBare[] =
    {
    3, /* tramsmit power level of the first entry */
    (uint8)(int8)-22, /* transmit power level of the last entry */
    /* 3 dBm */ 0xF5, /* characterized as 4.5 dBm in datasheet */
    /* 2 dBm */ 0xE5, /* characterized as 2.5 dBm in datasheet */
    /* 1 dBm */ 0xD5, /* characterized as 1 dBm in datasheet */
    /* 0 dBm */ 0xD5, /* characterized as 1 dBm in datasheet */
    /* -1 dBm */ 0xC5, /* characterized as -0.5 dBm in datasheet */
    /* -2 dBm */ 0xB5, /* characterized as -1.5 dBm in datasheet */
    /* -3 dBm */ 0xA5, /* characterized as -3 dBm in datasheet */
    /* -4 dBm */ 0x95, /* characterized as -4 dBm in datasheet */
    /* -5 dBm */ 0x95,
    /* -6 dBm */ 0x85, /* characterized as -6 dBm in datasheet */
    /* -7 dBm */ 0x85,
    /* -8 dBm */ 0x75, /* characterized as -8 dBm in datasheet */
    /* -9 dBm */ 0x75,
    /* -10 dBm */ 0x65, /* characterized as -10 dBm in datasheet */
    /* -11 dBm */ 0x65,
    /* -12 dBm */ 0x55, /* characterized as -12 dBm in datasheet */
    /* -13 dBm */ 0x55,
    /* -14 dBm */ 0x45, /* characterized as -14 dBm in datasheet */
    /* -15 dBm */ 0x45,
    /* -16 dBm */ 0x35, /* characterized as -16 dBm in datasheet */
    /* -17 dBm */ 0x35,
    /* -18 dBm */ 0x25, /* characterized as -18 dBm in datasheet */
    /* -19 dBm */ 0x25,
    /* -20 dBm */ 0x15, /* characterized as -20 dBm in datasheet */
    /* -21 dBm */ 0x15,
    /* -22 dBm */ 0x05 /* characterized as -22 dBm in datasheet */
    };

  • 你好!

         我按照你的方法,调用了函数都不可以,空旷距离不到10米(终端与协调器之间的距离),请问怎么解决呀?

        求大神指导!!!

    我用ZHA1.2.2协议栈:Z-Stack Home 1.2.2.42930,终端是endDeviceEB工程,CC2530芯片。

    以下是我调用两个地方,距离都是失败的。

    1、在int main( void )调用了不可以

    int main( void )

    {

    [.......]

    // Initialize the MAC
    ZMacInit();


    uint8 value=3;
    MAC_MlmeSetReq(MAC_PHY_TRANSMIT_POWER_SIGNED, &value);


    // Determine the extended address
    zmain_ext_addr();

    [.......]

    }

    2、

    在APP应用层zclSampleXXX_Init()初始化函数中调用也不可以。

  • 你直接使用下面的函数好了,

    uint8 ZMacSetTransmitPower( ZMacTransmitPower_t level );

    level TX_PWR_PLUS_5 

    这个函数可以放在应用层初始化的函数里。
    你要确定发射功率有没有正确配置的话,你可以调试模式下看下TXPOWER这个寄存器值
  • 你好!

        我使用ZMacSetTransmitPower()调试了,距离还是不超10米,距离不可以,

        硬件是网上买的开发板子,硬件不会有问题的。

        这个如何处理呀!?

        再次请大神们指教呀!

    TXPOWER的值为0XF5,我在调试模式下看到的。
    请看附件
     
    谢谢!
    注:协议栈ZHA1.2.2(Z-Stack Home 1.2.2.42930),CC2530芯片模块
  • 0xf5值是对的。剩下的你确定两步:

    1. 检查原理图,看控制PA的3个引脚分别是哪几个?是否于TI参考设计一致。

    2. 你可以用smartstudio直接控制,不需要写代码,用频谱仪测一下输出功率