This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

堆栈溢出如何处理

报警如下:Sat Jun 25 13:14:11 2016: The stack 'IdataStack' is filled to 100% (192 bytes used out of 192). The warning threshold is set to 90.%

Sat Jun 25 13:14:11 2016: The stack 'XdataStack' is filled to 100% (768 bytes used out of 768). The warning threshold is set to 90.%
Sat Jun 25 13:14:11 2016: The stack pointer for stack 'XdataStack' (currently XData:0xFFFF) is outside the stack range (XData:0x0001 to XData:0x0301)