This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Host APP通过UART连接ZNP Device失败

Other Parts Discussed in Thread: CC2630

请教下各位,我在CC2630上烧录ZNP程序,在Host主机上运行znp-host-framework程序,两者通过UART1接口(RX/TX/GND)直接进行通信。

使用的是UART without Power Management通信方式,但现在在Host主机上运行cmdLine.bin程序串口没有响应,提示下列信息:

# /opt/cmdLine.bin /dev/ttyS1
Do you wish to start/join a new network? (y/n)
y
rpcSendFrame: SRSP Error - CMD0: 0x21 CMD1: 0x09
network start failed
Network Error


rpcSendFrame: SRSP Error - CMD0: 0x21 CMD1: 0x04
rpcSendFrame: SRSP Error - CMD0: 0x21 CMD1: 0x09
Enter CMD

同样的测试,使用CC2650DK烧录ZNP程序,在Host主机上运行znp-host-framework程序,两者通过USB转串口连接进行通信,测试是成功的。
我比对了两者的UART连线,都是只使用了RX/TX/GND通信,差异貌似只有USB转接串口的差异。

是否是我有其他地方没有处理好,还请各位多多指教,谢谢!

x 出现错误。请重试或与管理员联系。