This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,现在在实际测试中发送这样的一个问题,Zstack2.5.1a版本的ZigBee协调器上,没法条件Zstack mesh1.1.0版本上开发的Router节点(这个节点目前是demo中的GenericAPP工程)。抓包显示情况是,入网过程全部正常,COO最后给router分配网络地址,整个入网过程完成,但是router感觉是没有存储这个节点信息,又再次发送入网请求。这个情况是否正常,还是这个router需要做一些配置???router能顺利加入到相同版本Zstack mesh1.1.0上的ZigBee协调器。谢谢。有知道的朋友回答下,谢谢
今天又仔细查了下,mesh1.1.0版本的Router,入网到版本为2.5.1A的COO下面,设备状态为DEV_END_DEVICE_UNAUTH。从而导致Router设备重启,然后重新入网,然后不断重复上述过程。能否有简单的方式避免上述情况,现在网络可能有上述2个版本的ZigBee节点。谢谢