Other Parts Discussed in Thread: CC2530, CC2630, CC2538
如题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OSAL.C里osal_run_system( void )这个函数就是处理所有事件的。
...
uint8 idx = 0;
do {
if (tasksEvents[idx]) // Task is highest priority that is ready.
{
break;
}
} while (++idx < tasksCnt);
...
这段意思就是idx从0号任务至tasksCnt号任务挨个找,哪个号有任务就break出去执行这个任务。
这个任务号顺序是固定的,如下:
const pTaskEventHandlerFn tasksArr[] = {
macEventLoop,
nwk_event_loop,
Hal_ProcessEvent,
#if defined( MT_TASK )
MT_ProcessEvent,
#endif
APS_event_loop,
#if defined ( ZIGBEE_FRAGMENTATION )
APSF_ProcessEvent,
#endif
ZDApp_event_loop,
#if defined ( ZIGBEE_FREQ_AGILITY ) || defined ( ZIGBEE_PANID_CONFLICT )
ZDNwkMgr_event_loop,
#endif
SAPI_ProcessEvent
};
const uint8 tasksCnt = sizeof( tasksArr ) / sizeof( tasksArr[0] );
可以看到macEventLoop是第一号任务,SAPI_ProcessEvent(用户应用)是最后一号任务;系统顺序查询这些任务号有没有需要执行的任务,这就是轮询。
不知道说明白没,你在研究下