我遇到一个奇葩问题,我的程序是这样的 P0_1 = 1; P0_5 = 0; powerSrcVoltage = HalAdcRead (HAL_ADC_CHANNEL_2, HAL_ADC_RESOLUTION_8);//只要加ADC采样这句话 P0_1, P0_5的配置好像就被AD的配置覆盖了,输出值都变成0了,如果把ADC注释掉就没问题,请问这怎么回事
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该没影响啊。建议提供下相关的代码。
HalAdcRead (HAL_ADC_CHANNEL_2, HAL_ADC_RESOLUTION_8)的函数如下:
uint16 HalAdcRead (uint8 channel, uint8 resolution)
{
int16 reading = 0;
#if (HAL_ADC == TRUE)
uint8 i, resbits;
uint8 adctemp;
volatile uint8 tmp;
uint8 adcChannel = 1;
uint8 reference;
/* store the previously set reference voltage selection */
reference = ADCCON3 & HAL_ADC_REF_BITS;
/*
* If Analog input channel is AIN0..AIN7, make sure corresponing P0 I/O pin is enabled. The code
* does NOT disable the pin at the end of this function. I think it is better to leave the pin
* enabled because the results will be more accurate. Because of the inherent capacitance on the
* pin, it takes time for the voltage on the pin to charge up to its steady-state level. If
* HalAdcRead() has to turn on the pin for every conversion, the results may show a lower voltage
* than actuality because the pin did not have time to fully charge.
*/
if (channel < 8)
{
for (i=0; i < channel; i++)
{
adcChannel <<= 1;
}
}
/* Enable channel */
ADCCFG |= adcChannel;
/* Convert resolution to decimation rate */
switch (resolution)
{
case HAL_ADC_RESOLUTION_8:
resbits = HAL_ADC_DEC_064;
break;
case HAL_ADC_RESOLUTION_10:
resbits = HAL_ADC_DEC_128;
break;
case HAL_ADC_RESOLUTION_12:
resbits = HAL_ADC_DEC_256;
break;
case HAL_ADC_RESOLUTION_14:
default:
resbits = HAL_ADC_DEC_512;
break;
}
/* read ADCL,ADCH to clear EOC */
tmp = ADCL;
tmp = ADCH;
/* Setup Sample */
adctemp = ADCCON3;
adctemp &= ~(HAL_ADC_CHN_BITS | HAL_ADC_DEC_BITS | HAL_ADC_REF_BITS);
adctemp |= channel | resbits | (reference);
/* writing to this register starts the extra conversion */
ADCCON3 = adctemp;
/* Wait for the conversion to be done */
while (!(ADCCON1 & HAL_ADC_EOC));
/* Disable channel after done conversion */
ADCCFG &= (adcChannel ^ 0xFF);
/* Read the result */
reading = (int16) (ADCL);
reading |= (int16) (ADCH << 8);
/* Treat small negative as 0 */
if (reading < 0)
reading = 0;
switch (resolution)
{
case HAL_ADC_RESOLUTION_8:
reading >>= 8;
break;
case HAL_ADC_RESOLUTION_10:
reading >>= 6;
break;
case HAL_ADC_RESOLUTION_12:
reading >>= 4;
break;
case HAL_ADC_RESOLUTION_14:
default:
reading >>= 2;
break;
}
#else
// unused arguments
(void) channel;
(void) resolution;
#endif
return ((uint16)reading);
}