This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIMAC1.5.2加入SerialBootloader后无法跳转到APP程序区

Other Parts Discussed in Thread: TIMAC

论坛大牛们,最近在用TIMAC1.5.2的库进行开发,加入bootloader,发现无法跳转到APP程序区,boot已经正常起来了,断点发现也已经执行到地址跳转指令。

   APP程序上,

chipcon_cstartup.s51用的是库里面的,本身包含了workaround.s51文件里面内容,如果不包含,在9.1版本以上的会报V1?V2?……错误。number of virtual值设置了为8了。

Iar版本只能用9.1以上版本打开,9.1版本和9.2版本都试了。

cc2530-sb.xcl用的是zSTACK2.5.1a里面的,

链接,生成bin文件命令也加了,

MAKE_CRC_SHDW的宏和_crcShdw也对照的改过了,

也选择了retain unchanged pages。但是就是无法跳转到app程序区。

但是如果是老版本的TIMAC就没有遇到这个问题了,与这些操作一样,但是可以跳转。