This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,排除处理器性能,无线通信部分CC2630提升的效果有多大。
发送,接收的指标提升不大,发送CC2530 4.5dbm,接收是-97dbm, CC2630 5dbm, 接收灵敏度是-100dbm
主要提升是功耗,cc2630几乎只有2530的1/3
另外,对比两者的抗干扰指标,selectivity和blocking, 2630确实有着不小的提升,可以对比数据手册看下。
谢谢,通过手册比较了了的确是这样的。那请问在组网性能上,2630相比2530有没什么提升吗。(比如在节点很多的情况下的传输性能方面)
没实测过,只是一些看法,供参考。
首先,如果你是用于zigbee标准的支持,传输速率,调制方式等都是一致的。从这个角度来看,传输性能不太可能有本质提升。M3核处理速度肯定更快,26系列还有专门的radio core(M0).,处理包,加密等那肯定要快很多。只是这对于节点很多的情况下,并不是说核快,发包就快,你发包,别的节点也发包,那就会冲突。速率是一定的,你总是需要一定时间才能发一个包。
射频处理 估计提高了2-5倍