This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530F256工作温度问题



现在用cc2530F256开发产品发现一个问题,就是通过下面函数获得芯片的工作电压,但是发现,随着温度的降低,监测的电压也随着变小,实际的供电电压是没有改变的,

static uint8 readVoltage(void)
{

uint16 value;

// Clear ADC interrupt flag
ADCIF = 0;

ADCCON3 = (0x00 | 0x10 | 0x0f);

// Wait for the conversion to finish
while ( !ADCIF );

// Get the result
value = ADCL;
value |= ((uint16) ADCH) << 8;


// value now contains measurement of Vdd/3
// 0 indicates 0V and 32767 indicates 1.25V
// voltage = (value*3*1.25)/32767 volts
// we will multiply by this by 10 to allow units of 0.1 volts
value = value >> 6; // divide first by 2^6
value = (uint16)(value * 34.5);
value = value >> 9; // ...and later by 2^9...to prevent overflow during multiplication

return value;

}

  • 您现在是使用电池供电的? 建议尝试以下操作

    1. 定义

      #define HAL_ADC_EOC 0x80 // End of Conversion bit
      #define HAL_ADC_START 0x40 // Starts Conversion
      #define HAL_ADC_RESOLUTION_8 0x01
      #define HAL_ADC_RESOLUTION_10 0x02
      #define HAL_ADC_RESOLUTION_12 0x03
      #define HAL_ADC_RESOLUTION_14 0x04
      #define HAL_ADC_CHN_VDD3 0x0f    // VDD/3
      #define HAL_ADC_REF_125V 0x00    // Internal Reference (1.15V for CC2530)

       
    2. 调用函数 uint16 sampledVoltage = adcRead( HAL_ADC_CHN_VDD3, HAL_ADC_RESOLUTION_12 );
       
    3.  使用 adcRead()

    uint16 adcRead (uint8 channel, uint8 resolution)

    {

    int16  reading = 0;

    uint8   i, resbits;

    uint8  adcChannel = 1;


    if (channel < 8)

    for (i=0; i < channel; i++)

    adcChannel <<= 1;


    /* Enable channel */

    ADCCFG |= adcChannel;


    /* Convert resolution to decimation rate */

    switch (resolution) {

    case HAL_ADC_RESOLUTION_8:

    resbits = HAL_ADC_DEC_064;

    break;


    case HAL_ADC_RESOLUTION_10:

    resbits = HAL_ADC_DEC_128;

    break;


    case HAL_ADC_RESOLUTION_12:

    resbits = HAL_ADC_DEC_256;

    break;


    case HAL_ADC_RESOLUTION_14:

    default:

    resbits = HAL_ADC_DEC_512;

    break;

    }


    /* writing to this register starts the extra conversion */

    ADCCON3 = channel | resbits | HAL_ADC_REF_125V;


    /* Wait for the conversion to be done */

    while (!(ADCCON1 & HAL_ADC_EOC));


    /* Disable channel after done conversion */

    ADCCFG &= (adcChannel ^ 0xFF);


    /* Read the result */

    reading = (int16) (ADCL);

    reading |= (int16) (ADCH << 8);


    /* Treat small negative as 0 */

    if (reading < 0)

    reading = 0;


    switch (resolution) {

    case HAL_ADC_RESOLUTION_8:

    reading >>= 8;

    break;


    case HAL_ADC_RESOLUTION_10:

    reading >>= 6;

    break;


    case HAL_ADC_RESOLUTION_12:

    reading >>= 4;

    break;


    case HAL_ADC_RESOLUTION_14:

    default:

    reading >>= 2;

    break;

    }

    return ((uint16)reading);

    }

  • 你好,测试了,还是不行,-20度,电压偏差有0.2v左右,常温下读值正确,温度低了就有偏差了

  • 你好,你的问题解决了吗?
  • 你好 在吗
    我也遇到类似低温的时候,产品工作不正常。
  • 不同溫度條件下的ADC讀值需要自行校正

  • 请您将问题详细描述后重新发帖,请不要跟踪旧贴,谢谢