Other Parts Discussed in Thread: Z-STACK, CC2530
TI大神你好,
目前我要实现通过串口来设置、修改节点的逻辑类型,目前使用的协议栈版本是ZStack-CC2530-2.3.0-1.4.0,请问这个协议栈可以实现这个功能么?如果不可以,请问需要使用哪些版本?问题比较急。。烦请帮忙解答~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没明白,我这边用了home1.2.2的在开发板上运行有问题,采用2.5.1版本的可以运行,但是系统一直在重启。现在决定还是采用ZStack-CC2530-2.3.0-1.4.0,我采用
zb_WriteConfiguration(ZCD_NV_LOGICAL_TYPE, sizeof(uint8), &u8temp);
osal_nv_item_init(ZCD_NV_LOGICAL_TYPE,1 ,NULL);
osal_nv_write(ZCD_NV_LOGICAL_TYPE ,0 ,1,&u8temp);
u8temp = ZCD_STARTOPT_AUTO_START;
zb_WriteConfiguration( ZCD_NV_STARTUP_OPTION, sizeof(uint8), &u8temp );
预编译了HOLD_AUTO_START,直接在设备类型的NV中写入启动类型,读取NV后确实改变了数据,但是系统重启后,不生效,仍旧按照配置文件里的类型执行,请问这种方法对吗?具体是怎样实现的?这个问题已经折磨四天了,希望有哪位可以帮帮忙,谢谢。
啊啊,解决了,小问题。。。
需要预编译BUILD_ALL_DEVICES,下面的就很容易操作了,就是上面用到的函数,采用ZStack-CC2530-2.3.0-1.4.0实现的