Other Parts Discussed in Thread: Z-STACK
我现在遇到的一个问题是这样的:一个网络有EndDevice100个,Router20个,同时上电,这样有时会出现coor下的节点都是EndDevice,导致Router不能入网,最后整个网络只有coor和21个EndDevice.
1、请问怎样才可以只允许Router连接到Coor?
2、有没有什么方法让EndDevic入网的时候只挑选Router作父节点?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于Zigbee 大规模组网,TI有一份专门的文档 http://www.ti.com/lit/an/swra427c/swra427c.pdf
建议您开启并使用MTO route
另外强烈不建议您同时给所有节点上电,建议随机上电
你好,请问networkDesc_t这个结构体是作什么用的?
typedef struct
{
uint16 panId;
byte logicalChannel;
byte routerCapacity;
byte deviceCapacity;
byte version;
byte stackProfile;
uint16 chosenRouter;
uint8 chosenRouterLinkQuality;
uint8 chosenRouterDepth;
uint8 extendedPANID[Z_EXTADDR_LEN];
byte updateId;
void *nextDesc;
} networkDesc_t;
我在NLMEDE.h中和z-stack API中都没有找到解释。 特别是chosenRouter这个参数是什么意思,是路由地址?
找到方法解决问题了,虽然有点不一样。
在void ZDO_beaconNotifyIndCB( NLME_beaconInd_t *pBeacon )中按照以下方法修改就可以了
//MSM:
#if defined ( RTR_NWK )
if ( (capacity) && (selected) ) //原代码
#else //添加的代码,禁止EndDevice保存Coor作为父节点入网
if ( (capacity) && (selected)&&( pBeacon->sourceAddr != 0x0000) )
#endif
//MSM
{
// this is the new chosen router for joining...
pNwkDesc->chosenRouter = pBeacon->sourceAddr;
pNwkDesc->chosenRouterLinkQuality = pBeacon->LQI;
pNwkDesc->chosenRouterDepth = pBeacon->depth;
}