This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack Mesh 1.0.0栈, 可周期睡眠的终端节点,程序不会进入睡眠中断函数,为何?

Other Parts Discussed in Thread: Z-STACK

        Z-Stack Mesh 1.0.0栈, 可周期睡眠的终端节点,周期5秒发送 data   request 数据,电流约50UA级别。

        但是程序不会进入 hal_sleep.c  文件的函数中断HAL_ISR_FUNCTION(halSleepTimerIsr, ST_VECTOR),我在HAL_ISR_FUNCTION(halSleepTimerIsr, ST_VECTOR)里面加调试用LED灯,发现LED灯不点亮,为何?

     在hal_sleep.c  文件 的void halSleepSetTimer(uint32 timeout)函数里面加调试LED是可以点亮的

  • 你好,你是怀疑节点在5s之间没有进入低功耗吗?

    一般办法你可以通过测量32MHz晶振的波形,可以判断设备有没有进入低功耗,

    另外一个办法你可以监测电流可以知道有没有进入低功耗。

  • vv你好

              我在做低功耗时看到这么一句话:“操作系统应用层(OSAL)在以1ms为最小定时单位的基础上,其最长定时时间为65秒”。也就是说使用osal_start_timerEx()最多只能休眠65s,不知道对不对。同时如果我想休眠500s,在应用层可不可直接控制睡眠寄存器。