协议栈默认支持4个led,我仿照例程添加了一个HAL_LED_5,单独测试HalLedSet ( HAL_LED_5, HAL_LED_MODE_OFF),HalLedSet ( HAL_LED_5, HAL_LED_MODE_ON)都可以,但是调用HalLedBlink( HAL_LED_5, 0, 50, 100 )没反应,求大神帮忙!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
协议栈默认支持4个led,我仿照例程添加了一个HAL_LED_5,单独测试HalLedSet ( HAL_LED_5, HAL_LED_MODE_OFF),HalLedSet ( HAL_LED_5, HAL_LED_MODE_ON)都可以,但是调用HalLedBlink( HAL_LED_5, 0, 50, 100 )没反应,求大神帮忙!
/***************************************************************************************************
* @fn HalLedBlink
* @brief Blink the leds
* @param leds - bit mask value of leds to be blinked
* numBlinks - number of blinks
* percent - the percentage in each period where the led will be on
* period - length of each cycle in milliseconds
* @return None
***************************************************************************************************/
建议改成HalLedBlink( HAL_LED_5, 5, 50, 200 )试试
是我疏忽了,还需要改以下值
#define HAL_LED_DEFAULT_MAX_LEDS 5
非常感谢耐心的解答!