This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 zstack串口透传解析

一、串口终端1的数据,如何被节点1所接收,并且发送出去的?

串口数据是由HAL层来负责的,让我们从主循环 (osal_start_system) 的Hal_ProcessPoll函数找下去 ,Hal_ProcessPoll ==> HalUARTPoll ==> HalUARTPollDMA。在这个 HalUARTPollDMA 函数里最后有这样一句话:dmaCfg.uartCB(HAL_UART_DMA-1,  evt); 对dmaCfg.uartCB 这个函数进行了调用,dmaCfg结构体类型如下:

typedef struct

{

  uint16 rxBuf[HAL_UART_DMA_RX_MAX];

  rxIdx_t rxHead;

  rxIdx_t rxTail;

  uint8 rxTick;

  uint8 rxShdw;

  uint8 txBuf[2][HAL_UART_DMA_TX_MAX];

  txIdx_t txIdx[2];

  volatile uint8 txSel;

  uint8 txMT;

  uint8 txTick;           // 1-character time in 32kHz ticks according to baud rate,

                          // to be used in calculating time lapse since DMA ISR

                          // to allow delay margin before start firing DMA, so that

                          // DMA does not overwrite UART DBUF of previous packet

  

  volatile uint8 txShdw;  // Sleep Timer LSB shadow.

  volatile uint8 txShdwValid; // TX shadow value is valid

  uint8 txDMAPending;     // UART TX DMA is pending

  halUARTCBack_t uartCB;
} uartDMACfg_t;

由上可知,uartCB是一个类型为halUARTCBack_t的函数指针(回调函数),那这个函数指针在那里赋值的呢?请看下面这条线路。void SerialApp_Init( uint8 task_id )里面有如下语句halUARTCfg_t uartConfig;在接下来的给uartConfig这个结构体变量赋值的语句中有如下语句:uartConfig.callBackFunc         = SerialApp_CallBack;即将uartConfig里的串口回调函数设置为SerialApp_CallBack,然后再通过HalUARTOpen (SERIAL_APP_PORT, &uartConfig);这个函数的调用(不再深入进去,有兴趣的同学可以进一步跟进)将uartConfig这个结构体变量的值转化为uartConfig这个结构体变量的值,注意两个结构体变量所属的类型不同,不能直接赋值,需要转化。

       这样就保证了,SerialApp_CallBack函数每次循环中被调用一次,SerialApp_CallBack( ) ==> SerialApp_Send( ),在SerialApp_Send()函数里会调用HalUARTRead()函数,将 DMA 数据读至数据 buffer 并通过 AF_DataRequest ()函数发送出去,注意:发送出去的信息的 CLUSTERID(信息簇ID)号为 SERIALAPP_CLUSTERID1。 

二、节点2 在收到空中的信号后,如何传递给与其相连的串口终端?
        节点 2 从空中捕获到信号后, 会应用层任务处理函数上进入AF_INCOMING_MSG_CMD分支,进入 SerialApp_ProcessMSGCmd()函数里进入处理。

void SerialApp_ProcessMSGCmd( afIncomingMSGPacket_t *pkt )  //对从空中捕获到的信号进行处理

{

  uint8 stat;

  uint8 seqnb;

  uint8 delay;

  switch ( pkt->clusterId )

  {

  // A message with a serial data block to be transmitted on the serial port.

  case SERIALAPP_CLUSTERID1:    //节点一发送过来的信息的 CLUSTERID(信息簇ID)号为 SERIALAPP_CLUSTERID1

    // Store the address for sending and retrying.

    osal_memcpy(&SerialApp_RxAddr, &(pkt->srcAddr), sizeof( afAddrType_t ));

    seqnb = pkt->cmd.Data[0];

    // Keep message if not a repeat packet

    if ( (seqnb > SerialApp_RxSeq) ||                    // Normal

        ((seqnb <</span> 0x80 ) && ( SerialApp_RxSeq > 0x80)) ) // Wrap-around

    {

      // Transmit the data on the serial port.

      if ( HalUARTWrite( SERIAL_APP_PORT, pkt->cmd.Data+1, (pkt->cmd.DataLength-1) ) )  //通过串口发送数据到PC机

      {

        // Save for next incoming message

        SerialApp_RxSeq = seqnb;

        stat = OTA_SUCCESS;

      }

      else

      {

        stat = OTA_SER_BUSY;

      }

    }

    else

    {

      stat = OTA_DUP_MSG;

    }

    // Select approproiate OTA flow-control delay.

    delay = (stat == OTA_SER_BUSY) ? SERIALAPP_NAK_DELAY : SERIALAPP_ACK_DELAY;

    // Build & send OTA response message.

    SerialApp_RspBuf[0] = stat;

    SerialApp_RspBuf[1] = seqnb;

    SerialApp_RspBuf[2] = LO_UINT16( delay );

    SerialApp_RspBuf[3] = HI_UINT16( delay );

    osal_set_event( SerialApp_TaskID, SERIALAPP_RESP_EVT );  //受到数据后,向节点1发送一个响应事件,跳到SerialApp_ProcessEvent()

    osal_stop_timerEx(SerialApp_TaskID, SERIALAPP_RESP_EVT);  

    break;

......

  }

}







UINT16 SerialApp_ProcessEvent( uint8 task_id, UINT16 events )  

{

......

   if ( events & SERIALAPP_RESP_EVT )    //串口响应事件,表示成功接受来自节点1的数据, 

  {

    SerialApp_Resp();      //向节点1发送  成功接受的response

    return ( events ^ SERIALAPP_RESP_EVT );

  }

......

}







static void SerialApp_Resp(void)

{

  if (afStatus_SUCCESS != AF_DataRequest(&SerialApp_RxAddr,         //通过AF_DataRequest函数,讲接收成功响应从空中发送出去

                                         (endPointDesc_t *)&SerialApp_epDesc,

                                          SERIALAPP_CLUSTERID2,
                                          SERIAL_APP_RSP_CNT, SerialApp_RspBuf,

                                         &SerialApp_MsgID, 0, AF_DEFAULT_RADIUS))

  {

    osal_set_event(SerialApp_TaskID, SERIALAPP_RESP_EVT);   //如果发送失败,重新发送

  }

}












节点1,接收到来自节点2的response。

UINT16 SerialApp_ProcessEvent( uint8 task_id, UINT16 events ) 

{

  ......

   while ( (MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( SerialApp_TaskID )) )

    {

      switch ( MSGpkt->hdr.event )

      {

         ......

         case AF_INCOMING_MSG_CMD:      //在这个实验中,使用串口通讯时,触发的事件,从空中捕获到信号。

            SerialApp_ProcessMSGCmd( MSGpkt );  //处理这个消息      

            break;

       ......

      }

    }

}

SERIALAPP_CLUSTERID2代表接收到发送成功的response,取消自动重发,如果不,自动重发。
void SerialApp_ProcessMSGCmd( afIncomingMSGPacket_t *pkt ) 
{
  ......
   // A response to a received serial data block.
  case SERIALAPP_CLUSTERID2:        //SerialWsn_CLUSTERID2代表接收到发送成功的response
    if ((pkt->cmd.Data[1] == SerialApp_TxSeq) &&
       ((pkt->cmd.Data[0] == OTA_SUCCESS) || (pkt->cmd.Data[0] == OTA_DUP_MSG)))
    {
      SerialApp_TxLen = 0;
      osal_stop_timerEx(SerialApp_TaskID, SERIALAPP_SEND_EVT);  //当收到发送成功的response,停止自动从发
    }
    else
    {
      // Re-start timeout according to delay sent from other device.
      delay = BUILD_UINT16( pkt->cmd.Data[2], pkt->cmd.Data[3] );
      osal_start_timerEx( SerialApp_TaskID, SERIALAPP_SEND_EVT, delay ); //没有收到成功的response,自动重发
    }
    break;
    default:
      break;
}



  • 下面部分来自网络上另一篇文章

    粗略的看了下这个程序,发现这个程序有一个EP(终端),每个终端有两个簇(SERIALAPP_CLUSTERID1、SERIALAPP_CLUSTERID2),可以在以下代码中定义

    // This list should be filled with Application specific Cluster IDs.
    const cId_t SerialApp_ClusterList[SERIALAPP_MAX_CLUSTERS] =
    {
    SERIALAPP_CLUSTERID1,
    SERIALAPP_CLUSTERID2
    };
    其中SERIALAPP_CLUSTERID1是负责数据的传输的,而SERIALAPP_CLUSTERID2则负责传输的反馈。在以下函数中可以看出

    void SerialApp_ProcessMSGCmd( afIncomingMSGPacket_t *pkt )
    
    {
    
      uint8 stat;
    
      uint8 seqnb;
    
      uint8 delay;
    
      switch ( pkt->clusterId )
    
      {
    
      // A message with a serial data block to be transmitted on the serial port.
    
      case SERIALAPP_CLUSTERID1:        // 处理数据
    
        // Store the address for sending and retrying.
    
        osal_memcpy(&SerialApp_RxAddr, &(pkt->srcAddr), sizeof( afAddrType_t ));  // 保存来信地址
    
        seqnb = pkt->cmd.Data[0];  // 保存计数(来自发送端,来用检验)
    
        // Keep message if not a repeat packet
    
        if ( (seqnb > SerialApp_RxSeq) ||                    // Normal, 是否是最新的数据
    
            ((seqnb <</span> 0x80 ) && ( SerialApp_RxSeq > 0x80)) ) // Wrap-around,
    
        {
    
    #ifndef   GEC_EP
    
          // Transmit the data on the serial port.
    
          if ( HalUARTWrite( SERIAL_APP_PORT, pkt->cmd.Data+1, (pkt->cmd.DataLength-1) ) )
    
          {
    
            // Save for next incoming message
    
            SerialApp_RxSeq = seqnb;   // 保存计数
    
            stat = OTA_SUCCESS;
    
          }
    
          else
    
          {
    
            stat = OTA_SER_BUSY;
    
          }
    
    #else                   // 添加部分代码,实现数据回传显示到串口,没办法串口只有一个
    
        if (afStatus_SUCCESS != AF_DataRequest(&SerialApp_RxAddr,
    
                                               (endPointDesc_t *)&SerialApp_epDesc,
    
                                                SERIALAPP_CLUSTERID1,
    
                                                SerialApp_TxLen+1, SerialApp_TxBuf,
    
                                                &SerialApp_MsgID, 0, AF_DEFAULT_RADIUS))
    
        {
    
          osal_set_event(SerialApp_TaskID, SERIALAPP_SEND_EVT);
    
        }
    
    #endif
    
        }
    
        else
    
        {
    
          stat = OTA_DUP_MSG;
    
        }
    
        // Select approproiate OTA flow-control delay.
    
        delay = (stat == OTA_SER_BUSY) ? SERIALAPP_NAK_DELAY : SERIALAPP_ACK_DELAY; // UART忙则延时16ms,否则延时1ms
    
        // Build & send OTA response message.
    
        SerialApp_RspBuf[0] = stat;   // 接收状态
    
        SerialApp_RspBuf[1] = seqnb;  // 计数
    
        SerialApp_RspBuf[2] = LO_UINT16( delay );
    
        SerialApp_RspBuf[3] = HI_UINT16( delay );
    
        osal_set_event( SerialApp_TaskID, SERIALAPP_RESP_EVT );  // 发送反馈信息
    
        osal_stop_timerEx(SerialApp_TaskID, SERIALAPP_RESP_EVT);  // 停止反馈定时器
    
        break;
    
      // A response to a received serial data block.
    
      case SERIALAPP_CLUSTERID2:    // 处理反馈
    
        if ((pkt->cmd.Data[1] == SerialApp_TxSeq) &&   // 反馈回来的是刚才发的
    
           ((pkt->cmd.Data[0] == OTA_SUCCESS) || (pkt->cmd.Data[0] == OTA_DUP_MSG)))  // 成功或者过期
    
        {
    
          SerialApp_TxLen = 0;    // 准备下一次发送
    
          osal_stop_timerEx(SerialApp_TaskID, SERIALAPP_SEND_EVT);  // 无需重发,关闭定时器
    
        }
    
        else   // 需要重发
    
        {
    
          // Re-start timeout according to delay sent from other device.
    
          delay = BUILD_UINT16( pkt->cmd.Data[2], pkt->cmd.Data[3] );    // 延时发送
    
          osal_start_timerEx( SerialApp_TaskID, SERIALAPP_SEND_EVT, delay );  //
    
        }
    
        break;
    
        default:
    
          break;
    
      }
    
    }
    

    总结一下以上的代码,当SERIALAPP_CLUSTERID1收到数据的时候,将会检验这个数据包是否是新的,由于逻辑有点复杂,下面用伪代码描述
    if (新数据包)

       if (UART发送成功)
       
            反馈成功信息;
         
        else  否则反馈UART忙;

    else 反馈此包过期;
    同样,对于SERIALAPP_CLUSTERID2的信息处理也可以这样描述
    if (刚才发送的包 && (成功 || 过期)) 
    {
       关闭定时器,注备下一次的发送,也就是说没有收到确认信息,不会进行下一次的发送
    }
    else
    {
      给我延时重发去
    }

  • 谢谢分享!也可以参考serial app

  • 哪里有:serial APP呢?