This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538光照传感器实验程序 并把光照值通过串口发送 ?

Other Parts Discussed in Thread: CC2538

CC2538光照传感器实验程序  并把光照值通过串口发送  帮忙看看哪里有错

#define EXAMPLE_PIN_UART_RXD GPIO_PIN_0
#define EXAMPLE_PIN_UART_TXD GPIO_PIN_1
#define EXAMPLE_GPIO_UART_BASE GPIO_A_BASE


#define EXAMPLE_PIN_I2C_SCL GPIO_PIN_2
#define EXAMPLE_PIN_I2C_SDA GPIO_PIN_3
#define EXAMPLE_GPIO_I2C_BASE GPIO_B_BASE

//*****************************************************************************
//
// Number of I2C data packets to send.
//
//*****************************************************************************
#define NUM_I2C_DATA 3

#define SLAVE_ADDRESS 0x46 

void
InitConsole(void)
{
//
// Map UART signals to the correct GPIO pins and configure them as
// hardware controlled.
//
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD,
IOC_MUX_OUT_SEL_UART0_TXD);
GPIOPinTypeUARTOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD);

IOCPinConfigPeriphInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD,
IOC_UARTRXD_UART0);
GPIOPinTypeUARTInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD);

//
// Initialize the UART (UART0) for console I/O.
//
UARTStdioInit(0);
}

//*****************************************************************************
//
// Configure the I2C0 master and slave and connect them using loopback mode.
//
//*****************************************************************************
int
main(void)
{
// uint32_t pui32DataTx[4]={2,3,4,5};
// uint32_t pui32DataRx[NUM_I2C_DATA];
//uint32_t ui32Index;
unsigned long delay;
unsigned short dis_data_0;
unsigned char i, BUF_0[8];
fp32 temp;

//
// Set the clocking to run directly from the external crystal/oscillator.
// (no ext 32k osc, no internal osc)
//
SysCtrlClockSet(false, false, SYS_CTRL_SYSDIV_16MHZ);

//
// Set IO clock to the same as system clock
//
SysCtrlIOClockSet(SYS_CTRL_SYSDIV_16MHZ);

//
// The I2C peripheral must be enabled before use.
//
SysCtrlPeripheralEnable(SYS_CTRL_PERIPH_I2C);

//
// Do reset of I2C module 执行I2C模块的复位
//
SysCtrlPeripheralReset(SYS_CTRL_PERIPH_I2C);

//
// Configure I2C pins 配置I2C引脚
//
GPIOPinTypeI2C(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SCL);
GPIOPinTypeI2C(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SDA);

//
// Configure pins as peripheral input and output 将引脚配置为外设输入和输出
//
IOCPinConfigPeriphInput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SCL,
IOC_I2CMSSCL);
IOCPinConfigPeriphInput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SDA,
IOC_I2CMSSDA);
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SCL,
IOC_MUX_OUT_SEL_I2C_CMSSCL);
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SDA,
IOC_MUX_OUT_SEL_I2C_CMSSDA);

//
// Enable loopback mode. Loopback mode is a built in feature that is
// useful for debugging I2C operations. It internally connects the I2C
// master and slave terminals, which effectively let's you send data as
// a master and receive data as a slave.
// NOTE: For external I2C operation you will need to use external pullups
// that are stronger than the internal pullups. Refer to the datasheet for
// more information.环回模式是一个内置功能,可用于调试I2C操作。
//它在内部连接I2C主机和从机端子,这有效地让您作为主机发送数据,并作为从机接收数据。
//注:对于外部I2C操作,需要使用比内部上拉电阻更强的外部上拉电阻。
HWREG(I2CM_CR) |= I2CM_CR_LPBK;

//
// Enable and initialize the I2C master module. Use the system clock for
// the I2C module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps. For this example we will use a data rate of 100kbps.
//启用并初始化I2C主模块。使用I2C模块的系统时钟。最后一个参数设置I2C数据传输速率。
//如果为false,则数据速率设置为100kbps,如果为true,则数据速率将设置为400kbps。
I2CMasterInitExpClk(SysCtrlClockGet(), false);
I2CMasterEnable();

//
// Enable the I2C slave module. This module is enabled only for testing
// purposes. It does not need to be enabled for proper operation of the
// I2Cx master module.使能I2C从模块。
//
I2CSlaveEnable(); // TBD is this needed or done by I2CSlaveInit

InitConsole();
// Place the data to be sent in the data register 将要发送的数据放在数据寄存器中
I2CMasterDataPut(0x01);
while(1)
{
I2CSlaveInit(SLAVE_ADDRESS);
I2CMasterSlaveAddrSet(SLAVE_ADDRESS, false);
I2CMasterDataPut(0x01);
I2CMasterDataPut(0x10);
delay = 1800000;
while(--delay);
I2CSlaveInit(SLAVE_ADDRESS+1);
I2CMasterSlaveAddrSet(SLAVE_ADDRESS+1, true);
/* // Do a dummy receive to make sure you don't get junk on the first receive.
//做一个虚拟接收,以确保你不会在第一次接收垃圾。
I2CMasterControl(I2C_MASTER_CMD_SINGLE_RECEIVE);
// Tell the master to read data.
I2CMasterControl(I2C_MASTER_CMD_SINGLE_RECEIVE); */

for (i=0; i<3; i++) //连续读取个地址数据,存储中BUF
{
BUF_0[i] = I2CMasterDataGet();
}


dis_data_0=BUF_0[0];
dis_data_0=(dis_data_0<<8)+BUF_0[1]; //合成数据,即光照数据
temp=(fp32)dis_data_0/1.2;

UARTprintf(" Sending: '%d' . . . ",temp);

}

帮忙看看哪里有错   谢谢了

  • 建议你单独调通一个模块,然后在合并。并且先找出问题,是发送部分的问题,还是读取传感器部分的问题。

  • 谢谢你  感觉这个iic程序是把主芯片 既做为主机又做为从机了  所以 I2CMasterDataGet()   I2CSlaveDataPut() I2CMasterDisable() 等iic.h中的函数可以用吗    要自己模拟写吗  还是可以用

  • 我觉得只要主从模式切换过来,还是可以用的。前提是你要切换ok。

  • #define uint32 unsigned int
    //
    //*****************************************************************************
    #define EXAMPLE_PIN_UART_RXD GPIO_PIN_0
    #define EXAMPLE_PIN_UART_TXD GPIO_PIN_1
    #define EXAMPLE_GPIO_UART_BASE GPIO_A_BASE


    #define EXAMPLE_PIN_I2C_SCL GPIO_PIN_2
    #define EXAMPLE_PIN_I2C_SDA GPIO_PIN_3
    #define EXAMPLE_GPIO_I2C_BASE GPIO_B_BASE

    //*****************************************************************************
    //
    // Number of I2C data packets to send.
    //
    //*****************************************************************************
    #define NUM_I2C_DATA 3

    //*****************************************************************************
    //
    // Set the address for slave module. This is a 7-bit address sent in the
    // following format:
    // [A6:A5:A4:A3:A2:A1:A0:RS]
    //
    // A zero in the "RS" position of the first byte means that the master
    // transmits (sends) data to the selected slave, and a one in this position
    // means that the master receives data from the slave.
    //
    //*****************************************************************************
    #define SLAVE_ADDRESS 0x46

    //*****************************************************************************
    //
    // This function sets up UART0 to be used for a console to display information
    // as the example is running.
    //
    //*****************************************************************************
    void start();
    void
    InitConsole(void)
    {
    //
    // Map UART signals to the correct GPIO pins and configure them as
    // hardware controlled.
    //
    IOCPinConfigPeriphOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD,
    IOC_MUX_OUT_SEL_UART0_TXD);
    GPIOPinTypeUARTOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD);

    IOCPinConfigPeriphInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD,
    IOC_UARTRXD_UART0);
    GPIOPinTypeUARTInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD);

    //
    // Initialize the UART (UART0) for console I/O.
    //
    UARTStdioInit(0);
    }

    //*****************************************************************************
    //
    // Configure the I2C0 master and slave and connect them using loopback mode.
    //
    //*****************************************************************************
    int
    main(void)
    {
    unsigned long delay;
    unsigned short dis_data_0;
    unsigned char i, BUF_0[8];
    uint32 vLux;
    fp32 temp;

    //
    // Set the clocking to run directly from the external crystal/oscillator.
    // (no ext 32k osc, no internal osc)
    //
    SysCtrlClockSet(false, false, SYS_CTRL_SYSDIV_16MHZ);

    //
    // Set IO clock to the same as system clock
    //
    SysCtrlIOClockSet(SYS_CTRL_SYSDIV_16MHZ);

    //
    // The I2C peripheral must be enabled before use.
    //
    SysCtrlPeripheralEnable(SYS_CTRL_PERIPH_I2C);

    //
    // Do reset of I2C module 执行I2C模块的复位
    //
    SysCtrlPeripheralReset(SYS_CTRL_PERIPH_I2C);

    //
    // Configure I2C pins 配置I2C引脚
    //
    GPIOPinTypeI2C(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SCL);
    GPIOPinTypeI2C(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SDA);

    //
    // Configure pins as peripheral input and output 将引脚配置为外设输入和输出
    //
    IOCPinConfigPeriphInput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SCL,
    IOC_I2CMSSCL);
    IOCPinConfigPeriphInput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SDA,
    IOC_I2CMSSDA);
    IOCPinConfigPeriphOutput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SCL,
    IOC_MUX_OUT_SEL_I2C_CMSSCL);
    IOCPinConfigPeriphOutput(EXAMPLE_GPIO_I2C_BASE, EXAMPLE_PIN_I2C_SDA,
    IOC_MUX_OUT_SEL_I2C_CMSSDA);

    //
    // Enable and initialize the I2C master module. Use the system clock for
    // the I2C module. The last parameter sets the I2C data transfer rate.
    // If false the data rate is set to 100kbps and if true the data rate will
    // be set to 400kbps. For this example we will use a data rate of 100kbps.
    //启用并初始化I2C主模块。使用I2C模块的系统时钟。最后一个参数设置I2C数据传输速率。
    //如果为false,则数据速率设置为100kbps,如果为true,则数据速率将设置为400kbps。
    I2CMasterInitExpClk(SysCtrlClockGet(), false);
    I2CMasterEnable();

    //
    // Enable the I2C slave module. This module is enabled only for testing
    // purposes. It does not need to be enabled for proper operation of the
    // I2Cx master module.使能I2C从模块。
    //
    I2CSlaveEnable(); // TBD is this needed or done by I2CSlaveInit???

    //
    // Set the slave address to SLAVE_ADDRESS. In loopback mode, it's an
    // arbitrary 7-bit number (set in a macro above) that is sent to the
    // I2CMasterSlaveAddrSet function.
    //
    I2CSlaveInit(SLAVE_ADDRESS);

    //
    // Tell the master module what address it will place on the bus when
    // communicating with the slave. Set the address to SLAVE_ADDRESS
    // (as set in the slave module). The receive parameter is set to false
    // which indicates the I2C Master is initiating a writes to the slave. If
    // true, that would indicate that the I2C Master is initiating reads from
    // the slave.
    //
    I2CMasterSlaveAddrSet(SLAVE_ADDRESS, false);


    //
    // Set up the serial console to use for displaying messages. This is
    // just for this example program and is not needed for I2C operation.
    InitConsole();
    // Place the data to be sent in the data register 将要发送的数据放在数据寄存器中
    // I2CMasterDataPut(0x46);
    //start();
    I2CMasterDataPut(0x10);
    start();
    I2CMasterDataPut(0x01);
    start();

    delay = 1800000;
    while(--delay);

    //I2CSlaveInit(SLAVE_ADDRESS+1);
    I2CMasterSlaveAddrSet(SLAVE_ADDRESS, true);
    // I2CMasterSlaveAddrSet(SLAVE_ADDRESS, true);
    // Do a dummy receive to make sure you don't get junk on the first receive.
    //做一个虚拟接收,以确保你不会在第一次接收垃圾。
    I2CMasterControl(I2C_MASTER_CMD_SINGLE_RECEIVE);

    //
    // Dummy acknowledge and wait for the receive request from the master.虚拟确认并等待来自主机的接收请求。
    // This is done to clear any flags that should not be set.
    //
    /* while(!(I2CSlaveStatus() & I2C_SLAVE_ACT_TREQ))
    {
    }*/
    // Do a dummy receive to make sure you don't get junk on the first receive.
    //做一个虚拟接收,以确保你不会在第一次接收垃圾。
    //I2CMasterControl(I2C_MASTER_CMD_SINGLE_RECEIVE);

    for (i=0; i<2; i++) //连续读取个地址数据,存储中BUF
    {
    BUF_0[i] = I2CMasterDataGet();
    }
    I2CMasterDataPut(0x00);
    start();
    // UARTprintf(" Sending: '%d' . . . ",BUF_0[0]);


    dis_data_0=BUF_0[0];
    dis_data_0=(dis_data_0<<8)+BUF_0[1]; //合成数据,即光照数据
    temp=(fp32)dis_data_0/1.2;
    vLux = (uint32)(temp*1.4);
    UARTprintf(" Sending: '%d' . . . ",vLux);
    //}
    }
    void start()
    {


    I2CMasterControl(I2C_MASTER_CMD_SINGLE_SEND);
    // Wait until the slave has received and acknowledged the data.
    while(!(I2CSlaveStatus() & I2C_SLAVE_ACT_RREQ))
    {
    }
    }

    这是修改过的  可以实现主机到从机发送数据  串口发送也是正常的  有一个问题是不能从从机寄存器里读出数据  望解答