大家好,打扰一下啊。现在做一个zigbee方面的电路,zigbee芯片选的是CC2420,控制芯片用的一个FPGA(要做一些算法)。现在的问题是,CC2420外挂的无源晶振不起振。对CC2420的初始化顺序是,先给VREG_EN管脚高电平,等待一段时间后再通过rst_n复位,等待一段时间后(百us级等待)写x"01"命令,也就是写寄存器选通命令SXOSCON(晶振打开命令),这时用示波器量测,晶振没有时钟输出。CC2420这个片子没有问题,命令也确定发进去了,因为对其它的寄存器采用写数据,再回读的方式,可以读到相同的数据。Vreg_out测的也是1.8V,无源晶振管脚连接对着芯片资料看了也是正确的。请问一下,还有什么问题可能导致晶振不起振啊?谢谢啊,麻烦了。