This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使能CHILD AGING后ZED周期性发出OrphanNotification是正常的吗?

Other Parts Discussed in Thread: Z-STACK, CC2530

协议栈:Z-Stack Home 1.2.2a

CPU:CC2530

请问,使能CHILD AGING后ZED周期性发出OrphanNotification是正常的吗?为什么呢?

(sniff文件见附件)

谢谢

period orphan notify when enable child agin.zip
  • 正常的,可以研究下协议栈下面的这段话。

    //======= Child Aging PARENT ROUTER (ZR/ZC) configuration ========
    // You can setup a router to support Child Table Aging in 1 of 2 modes of
    // operation. The first mode is NWK_PARENT_INFO_ORPHAN_NOTIFICATION and it
    // expects end devices to use orphan scan periodically as a means of a keep-alive
    // notification to the parent. The other mode is NWK_PARENT_INFO_MAC_DATA_POLL
    // which uses the end device's MAC POLL request as the keep-alive notification.
    // The first method is preferred for new devices, where the end devices provide
    // support for it (which will be manditory in future Zigbee Home Automation
    // Specifications).
    // The second method is compatible with older end devices without the need for
    // specific child aging support.
    //
    // The method supported by the router (or coordinator) is determined at build time
    // by setting zgNwkParentInformation to either NWK_PARENT_INFO_ORPHAN_NOTIFICATION
    // or NWK_PARENT_INFO_MAC_DATA_POLL.
    //
    // End device built with Child Table Aging support both methods, the method is
    // determined by the parent and communicated at run-time.
    #if ( ZG_BUILD_ENDDEVICE_TYPE )
    uint8 zgNwkParentInformation = NWK_PARENT_INFO_UNDEFINED;
    #else
    uint8 zgNwkParentInformation = NWK_PARENT_INFO_ORPHAN_NOTIFICATION;
    #endif

  • 根据这段解释请问我该如何去刷新age域呢?让终端发送ORPHAN_NOTIFICATION?为什么要用这种机制呢?按我的理解只要父节点收到终端的data request就会自动更新该终端的age域吧