This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 zigbee模块的在楼宇里测试传输距离是10米

Other Parts Discussed in Thread: CC2592

我们在楼宇里测试,发现CC2530 zigbee模块的传输距离是10米,中间只有单层玻璃门阻挡,而且玻璃门密封也不严实。是什么原因导致的?

另外,我还网上看到也有人说CC2530 zigbee模块在楼宇里的传输非常差(http://bbs.eeworld.com.cn/forum.php?mod=viewthread&tid=377509&page=1),是不是与我们提的产生原因相似?

还有,在空旷地带能否满足80-100米的稳定传输?

  • 玻璃门如果没有金属膜的话,对无线的衰减最多5dB

    所以10米应该是没有问题的。

    需要检查一下板子的天线和传导性能吧。在一个就是环境的2.4G干扰。

    BR.az

  • 据说增加CC2592,能跑到22db,不知道会不会提高发射功率和接收灵敏度,我们也在尝试

  • 解决步骤:

    1.模块是否有PA,没有的话问问厂家模块的发射功率,没有PA最大4.5db(3db),我实际测试,穿过一层楼板,10米差不多。

    2.自己做的模块的话,就得看天线的参数匹配了,是否做到最优,用抓吧工具可以模糊的测一下(相关仪器太贵)。

    3.程序如果是自己写的话也要注意功率设置。

    空旷地带的话如果是PCB天线 不带PA  80-100是极限,不能稳定。带PA的话,即使是再差,80-100最少可以90以上的稳定率。无线谈不上稳定传输。

    希望能有点小帮助。