Other Parts Discussed in Thread: Z-STACK
配置定时器1 模模式下,溢出中断,没有中断产出,总中断也开了,就是没有中断产生,该配置的也配置了,用的是z-stack的协议栈,哪里还有什么问题??
void HalTimer1Init (halTimerCBack_t cBack)
{
T1CCTL0 = 0; /* Make sure interrupts are disabled */
T1CCTL1 = 0; /* Make sure interrupts are disabled */
T1CCTL2 = 0; /* Make sure interrupts are disabled */
T1CCTL3 = 0; /* Make sure interrupts are disabled */
T1CCTL4 = 0; /* Make sure interrupts are disabled */
/* Setup prescale & clock for timer0 */
halTimerRecord[HW_TIMER_1].prescale = HAL_TIMER1_16_PRESCALE;
halTimerRecord[HW_TIMER_1].clock = HAL_TIMER_32MHZ;
halTimerRecord[HW_TIMER_1].prescaleVal = HAL_TIMER1_16_PRESCALE_VAL;
/* Setup Timer1 Channel structure */
halTimerChannel[HW_TIMER_1].TxCCTL = TCHN_T1CCTL;
halTimerChannel[HW_TIMER_1].TxCCL = TCHN_T1CCL;
halTimerChannel[HW_TIMER_1].TxCCH = TCHN_T1CCH;
halTimerChannel[HW_TIMER_1].TxOVF = TCNH_T1OVF;
halTimerChannel[HW_TIMER_1].ovfbit = TCHN_T1OVFBIT;
halTimerChannel[HW_TIMER_1].intbit = TCHN_T1INTBIT;
halTimerRecord[HW_TIMER_1].configured = TRUE;
halTimerRecord[HW_TIMER_1].opMode = HAL_TIMER1_OPMODE_MODULO;
halTimerRecord[HW_TIMER_1].channel = 0;
halTimerRecord[HW_TIMER_1].channelMode = HAL_TIMER_CH_MODE_OVERFLOW;
halTimerRecord[HW_TIMER_1].intEnable = TRUE;
halTimerRecord[HW_TIMER_1].callBackFunc = cBack;
//halTimerSetPrescale (HW_TIMER_3, halTimerRecord[HW_TIMER_3].prescale);
HalTimerStart (HAL_TIMER_3, 200000 );
}