Other Parts Discussed in Thread: TIMAC
1.采用basicrf的原因是客户有一个组建200多个节点的网络需求,采用zstack会有无法组织这么节点网络的问题。
2.由于这个组网的问题,确定采用basicrf的方式,借鉴点对点通信,可以猜想用一点对多点只要短地址事先分配好根据短地址就能实现组网
3.这样必须在系统中存在一个协调器,众多终端设被,而每个终端设备,也可以接受子节点,只要在程序中记录好子节点的短地址就好
4.为了维持这个稳定连接,以及运行过程中加入或者移除节点,就需要发送数据来确定当前的网络状态
问题:
1.首先这种1点对多点的情况采用basicrf是否合适,因为这样数据发送以及确认稳定连接的时候很有可能甚至是必然会发生冲突
2.论坛中有采用timac协议的说法,但是简单了解下似乎星形网络是一个协调器后接多个终端节点似乎和这个需求不太贴切。
3.如果采用basicrf合适,那么怎么样去解决数据冲突的问题